This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi together,
I bought recently an used MSP-FET430UIF from eBay and it seems it is faulty.
In Device Manager it appears as "MSP430 Application UART" but I get "MSP430.dll Initialization error". I tried on different 3 PCs (Windows XP, 7) with different versions of CCS, tried with Elprotronic Lite software and nothing. If it is seen by windows as "MSP430" device I guess the EEPROM contect is not altered so the MSP430F1612 could have a stuck firmware. I don't have another JTAG programmer to flash it. How can I flash it ? Is the BSL not deactivated on it ? I have 2 Launchpads if could help.
What I wanted to do with this FET is just to blow fuses. I was thinking about using the hardware part from "FET" in combination with LP in order to blow fuses over SBW.
Many thanks
Ionel Tiron said:Part Number: MSP-FET430UIF
Hi together,
I bought recently an used MSP-FET430UIF from eBay and it seems it is faulty.
In Device Manager it appears as "MSP430 Application UART" but I get "MSP430.dll Initialization error". I tried on different 3 PCs (Windows XP, 7) with different versions of CCS, tried with Elprotronic Lite software and nothing. If it is seen by windows as "MSP430" device I guess the EEPROM contect is not altered so the MSP430F1612 could have a stuck firmware. I don't have another JTAG programmer to flash it. How can I flash it ? Is the BSL not deactivated on it ? I have 2 Launchpads if could help.
What I wanted to do with this FET is just to blow fuses. I was thinking about using the hardware part from "FET" in combination with LP in order to blow fuses over SBW.
Many thanks
My LPa are EXP430G2 that has the same microcontroller F1612 like the FET UIF and same TUSB3410. What do you think if I exchange the F1612 ?
My FET UIF has 2 leds, Mode which is red and Power which is green. After connecting the USB cable the Mode led blinks 2 times and goes off followed by one turn on of green led which goes off also.
Many thanks
I am thinking about buying a new MSP FET but I have doubts:
1. Is capable a MSP-FET430UIF to blow the fuse over the SBW ?
2. Blowing the JTAG fuse over the SBW will disable also 4 wire JTAG ?
3. If I blow the fuse using 4 wires JTAG, could I use these pins for other stuff like I2C communication on P1.6 and P1.7 which are JTAG TDI and TDO ?
thanks
You didn't mention what is your target device. If your target device is from 5xx/6xx flash or FRAM family, than there is soft SBW/JTAG fuse that can be blown without applying VPP (6.5V), and any LP can do this. If you target device is from 2xx flash family than MSP-FET can generate VPP (6.5V) and blow the fuse. This can be done by SBW or JTAG. With blown fuse, SBW and JTAG access to device is disabled, but mailbox system (by SBW/JTAG) on 5xx/6xx flash and FRAM will work. JTAG port pins with blown fuse should work just fine. However, there is errata present on some devices, where state of this pins during boot code will not be in High-Z as it should be.
Does someone know if this programmer from Olimex can burn the real fuse over the SBW ?
Ionel Tiron said:
I read from different threads that there are people who didn't manage to blow the fuse on MSP430G2553 using MSP-FET430UIF or MSP - GANGpro and SBW.
Is there someone who managed to blow the fuse on MSP430G2 by SBW ? MSP430G2553 requires Vpp to be applied on the Test pin not on TDI.
I was thinking that someone from TI will give you clear answer on this, about blowing fuse on 2xx flash family by MSP-FET SBW.
Ionel Tiron said:Does someone know if this programmer from Olimex can burn the real fuse over the SBW ?
I guess that better place for correct answer will be on olimex forum, not here.
BTW, I will receive last hardware revision of my flasher at the end of the next week. Need some time for testing it. I see that you are in hurry, but I can PM you when I finish testing. Related web site will be finished next week. It is simple standalone software / hardware (MSP-GANG like) solution (not compatible with TI). It can blow 2xx fuse by SBW.
C:\msp430>flash -p com4 -e -fuse
Get Device
# JTID Fuse Device Proc
1 89 OK 2553 0060
Erase
Time: 63 ms
Fuse Blow (Y/N)? y
Release Device
Total Time: 2125 ms
C:\msp430>flash -p com4 -e
Get Device
# JTID Fuse
1 89 Blown
Error 101: Syncronization problem.
Release Device
Total Time: 47 ms
C:\msp430>
**Attention** This is a public forum