Other Parts Discussed in Thread: MAX232
Hi,
Can you please help me on the below question:
MSP430F5132 has one UART port ( UCA0TXD and UCA0RXD) and this port has been used.
1. Can i configure any other port pins as a UART? ( Need this additional port to interface my communication module) OR
2. Can i use a MAX232 device to create an another UART port?
MSP430 - GPIO pin --> MAX 232 device ---> communication module.
Thanks in advance.
Regards,
Rajesh.