Part Number: MSP430F2272
Hello Team,
I'm supporting a situation where a product based on the MSP430F2272 got released in the market but the AVss got not connected.
The team is working on doing a redesign to make sure that the problem is solved. The system is properly working but they want to better understand the failing scenarios in the field, so they have asked how the internal power supply pins are connected.
In particular the ADC is working even if the AVcc is not connected beside the AVss (also not connected).
As failing scenario/problem I do see the following:
- Without a good ground connection the analog peripheral may not get the specified datasheet values and are working out of specification (while they may be functional).
- The internal ESD diodes may not be properly working and the IO might get some over stress.
- 0.3V over Avcc or below AVss do not apply any longer since the ESD may not work properly.
Can you confirm the internal connection and failing scenarios?
Thanks,
SunSet