Part Number: MSP430FR5994
Other Parts Discussed in Thread: MSP-FET
Tool/software: Code Composer Studio
I have seen a number of posts about this error but can't seem to solve it. This only happens if my computer (Windows 7) goes to sleep. Then I have to re-boot, nothing else works. Simply unplugging the board and plugging it in again does not work. When they work everything is fine, just don't let it go to sleep. My USB ports are configured to not lose power (in the Device Manager the box for "Allow the computer to turn off this device to save power" is not checked). Is there a Windows override for this setting that ignores it?
I have two identical MSP430FR5994 on separate USB ports but it only seems to happen on one of them. I am using Code Composer Studio Version 7.3.0.00019. I have only had the boards for a couple months and I think the drivers are all the most recent.