Part Number: MSP430F4260
Other Parts Discussed in Thread: MSP430F5659, ADS1294,
Hi All,
I have error problem when using the TI download app, MSP430 USB Firmware Upgrade Example with data need to put in the information memory, infoD.
My chips is MSP430F5659, and my data in TI-TEXT file are:
@1800
FF AA
@8000
4F 14 F1 03 C1 43 00 00 E2 B2 3E 09 7A 24 B1 13
F6 6C C1 4C 00 00 E2 C2 3E 09 73 3C 03 43 C2 3C
03 43 C0 3C 03 43 BE 3C 92 B3 2C 53 BB 24 B1 13
24 84 C1 4C 00 00 B6 3C B1 13 38 65 A2 B3 2C 53
…
I don’t have error without the two line (@1800, FF AA). My code is:
case UPDATE_CODE_CMD:
ADS1294_Disable_Start();
// set starting BSL process
__disable_interrupt();
if (FCTL3 & LOCKA) {
FCTL3 = FWKEY | LOCKA;
}
else {
FCTL3 = FWKEY;
}
USBKEYPID = 0x9628;
USBCNF &= ~PUR_EN;
USBPWRCTL &= ~VBOFFIE;
USBKEYPID = 0x9600;
__delay_cycles(500000);
((void(*)())0x1000)(); // Call BSL
break;
Any idea to fix this problem?
Thanks,
Jack