This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Change 32kHz MSP430x2xx external timer

Hi,
We are using the MSP430x1xx series with an external 32.768 kHz crystal, but for our application the times given by this crystal are not enough. We need a timer that triggers every 16us. 
We have seen that with the MSP430x2xx series is possible to change the clock source of 32.768 kHz with another in the 400kHz to 16 MHz range using the LFXT1CLK with the HF mode enabled, is it correct? Are there some test with different clock sources like http://www.ti.com/lit/pdf/slaa225 for the 32.768 kHz?
Thanks in advance

**Attention** This is a public forum