Tool/software: Code Composer Studio
I want to multiply two ADC readings (voltage and current to get power). I am using CCS7 version and I enabled the hardware multiplier in CCS project properties, compiler and linker(set to 16).
But the result in the watch window is nowhere near the actual answer. If I try to multiply two variables, the result i am getting is '314' for any value of the variables. And if try to multiply one variable(value 45) with a constant, i can not increase the value of the constant more than the number 32, when ever it goes more than 32, the result becomes '314'. If I multiply two constant numbers, whose product is less than 32768, i am getting the right answer.
Am I missing any settings..??
The variable declaration and multiplication portion is as given below
unsigned int adc_val[6]={0,0,0,0,0,0};
unsigned int v_pan_avg_acc_n10=0,c_pan_avg_acc_n10=0,v_pan_avg_n7=0,c_pan_avg_n7=0;
unsigned int panel_pwr_n14=0;
------------------------------------------------------
-----------------------------------------------------
v_pan_avg_acc_n10 = v_pan_avg_acc_n10+adc_val[4];
c_pan_avg_acc_n10 = c_pan_avg_acc_n10+adc_val[1];
adc_count++;
if(adc_count>32)
{
v_pan_avg_n7 = v_pan_avg_acc_n10>>8;
....................................................................
c_pan_avg_n7 = c_pan_avg_acc_n10>>8;
panel_pwr_n14 = (v_pan_avg_n7) * (c_pan_avg_n7 );
..................................................................
.................................................................
}