Part Number: MSP430FR5869
Hi:
I'm using ADC12 in Repeat-signal-channel mode,the ADC12SHSx is 0, the clock source is SMCLK which is 8Mhz and adc clock divider is 1MHz.
And I'm using DMA to transfer adc result, the low power mode is LPM3.
For most time, the MCU works fine, but sometime it stoped.
In debug mode, I find ADC12 stop convert with ADC12SC keep 1 (datasheet says ADC12SC is reset automatically), ADC12BUSY keep 1,
and DMA doesn't transfer any data.
Can anyone help me solve this problem? thanks very much!