Part Number: MSP430FR5739
I am trying to determine why I am seeing greater than expected latency when polling a GPIO input and setting a GPIO output during a polling loop. ( NOTE: I realize polling an input in this manner is generally a no-no; but for sake of this discussion, take the code below as-is ) For the record, I can't find a definitive measure of how long it takes to read a pin and then set a GPIO based on the status of that pin. Anyway...
Clock system is setup to accept a 16MHz from a TCXO on XIN.
P2.3 is attached to a signal generator, 10Hz @10% duty cycle.
P2.3 is setup as an input with pulldown resistor enabled. Pin 1.0 is setup as an output. Between when P2.3 goes high ( button push ) and P1.0 I am seeing a latency of 620ns. Since my MCLK period is 62.5ns it takes about 9 MCLK cycles to read the pin and set P1.0. This seems excessive to me and I cannot figure out if what I am seeing is the expected behavior.
#include <msp430fr5739.h>
// Prototypes
void initCS(void);
void initGPIO(void);
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
initCS();
initGPIO();
__delay_cycles(100);
while(1){
if( P2IN & BIT3 ) // If P2.3 went high ...
{
P1OUT |= BIT0; // ... set P1.0 high immediately
}
}//while(1)
return 0;
}//main()
void initCS(void)
{
PJSEL0 |= BIT4; // Set PJ.4 as XIN, digital square wave input
PJSEL1 &= ~BIT4;
CSCTL0_H = 0xA5; // Unlock password for updating CS
//CSCTL1 |= // Don't care about this register, not using DCO
CSCTL2 = SELM__XT1CLK + SELS__XT1CLK + SELA__XT1CLK; // MCLK source = XT1CLK; SMCLK source = XT1CLK;
// ACLK source = XT1CLK
CSCTL3 = DIVM__1 + DIVS__2 + DIVA__32; // MCLK/1; SMCLK/2; ACLK/32
CSCTL4 |= XT1BYPASS | XTS | XT2OFF; // Select Bypass mode operation
// for XT1; select high-freq. mode;
// Don't need XT2 so turn it off
do
{
CSCTL5 &= ~XT1OFFG; // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
__delay_cycles(10000); // Wait around a little while before next check
} while (SFRIFG1&OFIFG); // Test oscillator fault flag
PJDIR |= BIT5; // Set PJ.5 as a GPIO output ( don't need XOUT )
PJDIR |= BIT0; // Set PJ.0 as SMCLK output
PJSEL0 |= BIT0;
PJSEL1 &= ~BIT0;
PJDIR |= BIT1; // Set PJ.1 as MCLK output
PJSEL0 |= BIT1;
PJSEL1 &= ~BIT1;
PJDIR |= BIT2; // Set PJ.2 as ACLK output
PJSEL0 |= BIT2;
PJSEL1 &= ~BIT2;
}//initCS()
void initGPIO(void)
{
// Pulse output pin P1.0
P1DIR |= BIT0; // Set P1.0 as an output pin
P1OUT &= ~BIT0; // Initialize P1.0 to low
// Sync sensing pin P2.3
P2DIR &= ~BIT3; // Set P2.3 as an input pin
P2REN |= BIT3; // Enable pu or pd on this pin
P2OUT &= ~BIT3; // Select pull-down resistor on this pin
__delay_cycles(5); // Give time for pullup to settle
}
(1) Do compiler settings ( DEBUG vs. RELEASE mode ) have anything to do with this latency?
(2) Is there a way to lower this latency?
(3) For the record, using an interrupt to set P1.0 results in even greater latency between P2.3 going high and P1.0 going high.