Tool/software: Code Composer Studio
Hello all,
I am using the MSP-EXP430FR5739 experimenter board for an embedded systems course I am teaching. I had no trouble getting the serial communication to work on my home windows laptop running Windows 8.1, but have been having considerable issues achieving a consistent serial port connection on our lab computers running Windows 10. They are all running Code Composer 7.2, and have no problem flashing code, but the serial port is inconsistent. I have only been able to get the serial connection to work for a few minutes at a time. At one point I uninstalled code composer and the serial connection worked great. Then I couldn't get it to work again even after reinstalling and uninstalling a second time. I've tried restarting computers/code composer/serial connection/board in various configurations, and no dice. If I have trouble connecting on my windows machine I can always get it to work in one or two resets of the serial terminal. EDIT: I should clarify that on the lab computers, I am able to open the serial port, but the port does not receive characters from the experimenter board. I have confirmed characters are being transmitted with a scope.
I did some digging and I have been trying to research solutions. this thread suggested usb 3.0 ports could be an issue. The computers appear to have usb 3.0 ports (blue), but also what appear to be standard black ports. Is there a way to confirm they are in fact USB 2.0 ports? Could using a computer with any usb 3.0 ports be an issue?
One thing I noticed is that the COM ports are high (21 or so). Could that be an issue?
Are there other things I'm missing?
Students who have installed CCS on their laptops seem to be having fewer issues, but I can't say for sure whether it's only an issue with the lab computers as we've only just started this lab.
Thank you!