This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5528: Time measurement

Part Number: MSP430F5528

Hi,

I want to measure the time interval between transmitting and receiving and show it on a lcd. I have written a code that enables the timer 0 when a data is transmitting and stops the timer when a data is received. Then copies the TA0R value to lcd. Every time it is showing the data but that are some random values. I am inserting my code here . If there any problem then guide me.

#include <msp430.h>

#define DR P4OUT = P4OUT | BIT1 // define RS high
#define CWR P4OUT = P4OUT & (~BIT1) // define RS low
#define READ P4OUT = P4OUT | BIT2 // define Read signal R/W = 1 for reading
#define WRITE P4OUT = P4OUT & (~BIT2) // define Write signal R/W = 0 for writing
#define ENABLE_HIGH P1OUT = P1OUT | BIT4 // define Enable high signal
#define ENABLE_LOW P1OUT = P1OUT & (~BIT4) // define Enable Low signal
unsigned int i;
unsigned int j;

void delay(unsigned int k)
{
for(j=0;j<=k;j++)
{
for(i=0;i<100;i++);
}
}
void data_write(void)
{
ENABLE_HIGH;
delay(2);
ENABLE_LOW;
}
void data_read(void)
{
ENABLE_LOW;
delay(2);
ENABLE_HIGH;
}
void check_busy(void)
{
PJDIR &= ~(BIT3); // make P1.3 as input
while((PJIN&BIT3)==1)
{
data_read();
}
PJDIR |= BIT3; // make P1.3 as output
}
void send_command(unsigned char cmd)
{
check_busy();
WRITE;
CWR;
PJOUT = (PJOUT & 0xF0)|((cmd>>4) & 0x0F); // send higher nibble
data_write(); // give enable trigger
PJOUT = (PJOUT & 0xF0)|(cmd & 0x0F); // send lower nibble
data_write(); // give enable trigger
}
void send_data(unsigned int data)
{
check_busy();
WRITE;
DR;
PJOUT = (PJOUT & 0xF0)|((data>>4) & 0x0F); // send higher nibble
data_write(); // give enable trigger
PJOUT = (PJOUT & 0xF0)|(data & 0x0F); // send lower nibble
data_write(); // give enable trigger
}
void send_string(char*s)
{
while(*s)
{
send_data(*s);
s++;
}
}
void lcd_init(void)
{
PJDIR |= 0xFF;
PJOUT &= 0x00;
P4DIR |= 0xFF;
P4OUT &= 0x00;
P1DIR |= 0xFF;
P1OUT &= 0x00;
send_command(0x33);
send_command(0x32);
send_command(0x28); // 4 bit mode
send_command(0x0E); // clear the screen
send_command(0x01); // display on cursor on
send_command(0x06); // increment cursor
send_command(0x80); // row 1 column 1
}


int data;
int main(void)
{
  WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
  P4SEL = BIT4+BIT5;                        // P3.4,5 = USCI_A0 TXD/RXD
  UCA1CTL1 |= UCSWRST;                      // **Put state machine in reset**
  UCA1CTL1 |= UCSSEL_2;                     // SMCLK
  UCA1BR0 = 6;                              // 1MHz 9600 (see User's Guide)
  UCA1BR1 = 0;                              // 1MHz 9600
  UCA1MCTL = UCBRS_0 + UCBRF_13 + UCOS16;   // Modln UCBRSx=0, UCBRFx=0,
                                            // over sampling
  UCA1CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**

  UCA1IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt
  while (!(UCA1IFG&UCTXIFG));             // USCI_A0 TX buffer ready?
            UCA1TXBUF = 53;                  // TX -> RXed character
  __bis_SR_register(LPM0_bits + GIE);       // Enter LPM0, interrupts enabled
  __no_operation();                         // For debugger
}

// Echo back RXed character, confirm TX buffer is ready first
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A1_VECTOR
__interrupt void USCI_A1_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A1_VECTOR))) USCI_A1_ISR (void)
#else
#error Compiler not supported!
#endif
{
  switch(__even_in_range(UCA1IV,4))
  {
  case 0:break;                             // Vector 0 - no interrupt
  case 2:
      TA0CTL = MC__STOP;
     data = TA0R; // Vector 2 - RXIFG
     lcd_init();
     send_data(data);
      while (!(UCA1IFG&UCTXIFG));             // USCI_A0 TX buffer ready?
         UCA1TXBUF = UCA1RXBUF;                  // TX -> RXed character
         TA0CCR0 = 65535;
          TA0CTL = TASSEL_2 + MC_1 + TACLR;         // SMCLK, upmode, clear TAR
    break;
  case 4:

      break;                             // Vector 4 - TXIFG
  default: break;
  }
}




Thanks...

Pabel

**Attention** This is a public forum