Part Number: MSP-EXP430FR5739
Other Parts Discussed in Thread: MSP430FR5739,
Tool/software: Code Composer Studio
Pulling my hair out over this one.
Wrote a simple blinky led program to test IO. Start debug session a few times in a row, enters and exists debug just fine. All of a sudden, debug sessions will not start. CCS freezes on the screen:
Plugging/unplugging the USB cable to the Launchpad does not help; CCS remains frozen in this state. Restarting CCS fixes the issue about 50% of the time, other 50% of the time, same issue occurs again and again and again. Sometimes the error message is different, referring to "Could not perform soft reset" and about writing to a memory location:
I've used dozens of Launchpads on this same system, without fail. Only difference with the EXP-430FR5789 is that is is an old style Mini-USB connector onto the Launchpad. I can't imagine why that would matter. Anybody have an idea of what's going on here?