This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5132: UCB0 SPI Problem

Part Number: MSP430F5132


Tool/software: Code Composer Studio

Hello,

I couldnt get any response from the SPI channel of MSP430F5132. Here is the info of my application:

1) There is no output at MOSI pin. 

2) Codes:

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>main.c <<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<

#include <string.h>
#include <stdio.h>
#include <stdlib.h>
#include "driverlib.h"
#include "msp430_spi.h"


char charArray[20],charArrayID[6],cbuf1[1],cbuf2[1],cbuf3[1],cbuf4[1],cbuf5[1],cbuf6[1],cbuf7[1],cbuf8[1],cbuf9[1],cbuf10[1],cbuf11[1],cbuf12[1],cbuf13[1],cbuf14[1],cbuf15[1],cbuf16[1];
volatile int i,c=0;
uint8_t receivedData = 0x00,buf1,buf2,buf3,buf4,buf5,buf6,buf7,buf8,buf9,buf10,buf11,buf12,buf13,buf14,buf15,buf16;
//uint8_t buf[16];


void main (void)
{
    //Stop WDT
    WDT_A_hold(WDT_A_BASE);

    //STATUS1 STATUS2 output
    GPIO_setAsOutputPin(GPIO_PORT_P3,GPIO_PIN0 + GPIO_PIN1);
    //STATUS1 STATUS2 low
    GPIO_setOutputLowOnPin(GPIO_PORT_P3,GPIO_PIN0 + GPIO_PIN1);

    //rs485 de re
    GPIO_setAsOutputPin(GPIO_PORT_P2, GPIO_PIN0 + GPIO_PIN1);
    //re de low
    GPIO_setOutputLowOnPin(GPIO_PORT_P2, GPIO_PIN0 + GPIO_PIN1);

    //uart - rs485
    GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1, GPIO_PIN1 + GPIO_PIN2);

    //spi - ste = p1.0
    spi_init();
    GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0);// + GPIO_PIN3 + GPIO_PIN4 + GPIO_PIN5);
    GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);// + GPIO_PIN3 + GPIO_PIN4 + GPIO_PIN5);
    //GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);



    //Baudrate = 9600, clock freq = 1.048MHz
    //UCBRx = 109, UCBRFx = 0, UCBRSx = 2, UCOS16 = 0  --> Copied from MSP430F5529 example
    USCI_A_UART_initParam param = {0};
    param.selectClockSource = USCI_A_UART_CLOCKSOURCE_SMCLK;
    param.clockPrescalar = 109;
    param.firstModReg = 0;
    param.secondModReg = 2;
    param.parity = USCI_A_UART_NO_PARITY;
    param.msborLsbFirst = USCI_A_UART_LSB_FIRST;
    param.numberofStopBits = USCI_A_UART_ONE_STOP_BIT;
    param.uartMode = USCI_A_UART_MODE;
    param.overSampling = USCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION;

    if(STATUS_FAIL == USCI_A_UART_init(USCI_A0_BASE, &param))
    {
        return;
    }

    //Enable UART module for operation
    USCI_A_UART_enable(USCI_A0_BASE);

    //Enable Receive Interrupt
    USCI_A_UART_clearInterrupt(USCI_A0_BASE,USCI_A_UART_RECEIVE_INTERRUPT);
    USCI_A_UART_enableInterrupt(USCI_A0_BASE,USCI_A_UART_RECEIVE_INTERRUPT);


    //CIHAZ ID
    charArrayID[0] = '4';
    charArrayID[1] = '6';
    charArrayID[2] = '0';
    charArrayID[3] = '7';
    charArrayID[4] = '5';
    charArrayID[5] = '1';



    //ads8684 ayarlar
    ///reset
    GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
    //__delay_cycles(1000);
    spi_transfer16(0x8500);
    GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
    __delay_cycles(1000);

    //AUTO_SEQ_EN
    GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
    __delay_cycles(1000);
    spi_transfer16(0x01FF);
    GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
    __delay_cycles(1000);


    //CHANNEL POWER DOWN -> ALL UP
    /*GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
    __delay_cycles(1000);
    spi_transfer16(0x0200);
    GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
    __delay_cycles(1000);*/


    //channel 1 2.5xVref
    GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
    //__delay_cycles(1000);
    spi_transfer16(0x0505);
    GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
    __delay_cycles(1000);

    //channel 2 2.5xVref
    GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
    //__delay_cycles(1000);
    spi_transfer16(0x0605);
    GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
    __delay_cycles(1000);

    //channel 3 2.5xVref
    GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
    //__delay_cycles(1000);
    spi_transfer16(0x0705);
    GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
    __delay_cycles(1000);

    //channel 4 2.5xVref
    GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
    //__delay_cycles(1000);
    spi_transfer16(0x0805);
    GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
    __delay_cycles(1000);

    GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
    //__delay_cycles(1000);
    spi_transfer16(0xA000);
    spi_transfer16(0x0000);
    GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
    __delay_cycles(1000);




    __enable_interrupt();

    while(1){
        GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
        GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN1);
        __delay_cycles(105000);
        GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN1);
        GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
        __delay_cycles(105000);

        __disable_interrupt();



        //CH1
        GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
        //__delay_cycles(10000);
        buf1 = spi_transfer(0x00);
        buf2 = spi_transfer(0x00);
        buf3 = spi_transfer(0x00);
        buf4 = spi_transfer(0x00);
        GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
        __delay_cycles(10000);
        //CH2
        GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
        //__delay_cycles(10000);
        buf5 = spi_transfer(0x00);
        buf6 = spi_transfer(0x00);
        buf7 = spi_transfer(0x00);
        buf8 = spi_transfer(0x00);
        GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
        __delay_cycles(10000);
        //CH3
        GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
        //__delay_cycles(10000);
        buf9 = spi_transfer(0x00);
        buf10 = spi_transfer(0x00);
        buf11 = spi_transfer(0x00);
        buf12 = spi_transfer(0x00);
        GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
        __delay_cycles(10000);
        //CH4
        GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
        //__delay_cycles(10000);
        buf13 = spi_transfer(0x00);
        buf14 = spi_transfer(0x00);
        buf15 = spi_transfer(0x00);
        buf16 = spi_transfer(0x00);
        GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
        __delay_cycles(10000);

        ltoa(buf1, cbuf1);
        ltoa(buf2, cbuf2);
        ltoa(buf3, cbuf3);
        ltoa(buf4, cbuf4);
        ltoa(buf5, cbuf5);
        ltoa(buf6, cbuf6);
        ltoa(buf7, cbuf7);
        ltoa(buf8, cbuf8);
        ltoa(buf9, cbuf9);
        ltoa(buf10, cbuf10);
        ltoa(buf11, cbuf11);
        ltoa(buf12, cbuf12);
        ltoa(buf13, cbuf13);
        ltoa(buf14, cbuf14);
        ltoa(buf15, cbuf15);
        ltoa(buf16, cbuf16);

        buf1 = 0;
        buf2 = 0;
        buf3 = 0;
        buf4 = 0;
        buf5 = 0;
        buf6 = 0;
        buf7 = 0;
        buf8 = 0;
        buf9 = 0;
        buf10 = 0;
        buf11 = 0;
        buf12 = 0;
        buf13 = 0;
        buf14 = 0;
        buf15 = 0;
        buf16 = 0;




        GPIO_setOutputHighOnPin(GPIO_PORT_P2, GPIO_PIN0 + GPIO_PIN1);
        __delay_cycles(18000);

        USCI_A_UART_transmitData(USCI_A0_BASE, 'A');
        USCI_A_UART_transmitData(USCI_A0_BASE, 'C');
        USCI_A_UART_transmitData(USCI_A0_BASE, 'K');
        USCI_A_UART_transmitData(USCI_A0_BASE, charArrayID[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, charArrayID[1]);
        USCI_A_UART_transmitData(USCI_A0_BASE, charArrayID[2]);
        USCI_A_UART_transmitData(USCI_A0_BASE, charArrayID[3]);
        USCI_A_UART_transmitData(USCI_A0_BASE, charArrayID[4]);
        USCI_A_UART_transmitData(USCI_A0_BASE, charArrayID[5]);
        USCI_A_UART_transmitData(USCI_A0_BASE, '#');
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf1[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf2[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf3[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf4[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, '#');
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf5[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf6[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf7[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf8[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, '#');
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf9[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf10[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf11[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf12[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, '#');
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf13[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf14[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf15[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, cbuf16[0]);
        USCI_A_UART_transmitData(USCI_A0_BASE, '\n');



        __delay_cycles(18000);
        GPIO_setOutputLowOnPin(GPIO_PORT_P2, GPIO_PIN0 + GPIO_PIN1);
        __enable_interrupt();
    }
}

//******************************************************************************
//
//This is the USCI_A0 interrupt vector service routine.
//
//******************************************************************************


#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(USCI_A0_VECTOR)))
#endif
void USCI_A0_ISR(void)
{
    switch(__even_in_range(UCA0IV,4))
    {
    //Vector 2 - RXIFG
    case 2:
        receivedData = USCI_A_UART_receiveData(USCI_A0_BASE);

        /*if(receivedData != '#')                       // Check value
        {
            if((c == 0 && receivedData == '4') || (c == 1 && receivedData == '6') || (c == 2 && receivedData == '0') || (c >= 3 && c < 13) )
            {
                charArray[c] = receivedData;
                c++;
                charReceived = 0;
            }else
            {
                c = 0;
                charReceived = 0;
            }
        }else{
            //c = 0;
            //GPIO_toggleOutputOnPin(GPIO_PORT_P7, GPIO_PIN1);
            charReceived = 1;
        }*/
        break;
    default: break;
    }
}

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>msp430_spi.c <<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<

#if defined(__MSP430_HAS_USCI_B0__) && defined(SPI_DRIVER_USCI_B)
void spi_init()
{
	/* Configure ports on MSP430 device for USCI_B */
	#ifdef __MSP430F5172
	P1SEL |= BIT3 | BIT4 | BIT5;
	#endif
	#ifdef __MSP430F5529
	P3SEL |= BIT0 | BIT1 | BIT2;
	#endif
    #ifdef __MSP430F5132
    P1SEL |= BIT3 | BIT4 | BIT5;
    #endif

	/* USCI-B specific SPI setup */

	UCB0CTL1 |= UCSWRST;
	UCB0CTL0 = UCCKPH | UCMSB | UCMST | UCMODE_0 | UCSYNC;  // SPI mode 0, master
	UCB0BR0 = 0x01;  // SPI clocked at same speed as SMCLK
	UCB0BR1 = 0x00;
	UCB0CTL1 = UCSSEL_2;  // Clock = SMCLK, clear UCSWRST and enables USCI_B module.


}

uint8_t spi_transfer(uint8_t inb)
{
	UCB0TXBUF = inb;
	while ( !(UCB0IFG & UCRXIFG) )  // Wait for RXIFG indicating remote byte received via SOMI
		;
	return UCB0RXBUF;
}

uint16_t spi_transfer16(uint16_t inw)
{
	uint16_t retw;
	uint8_t *retw8 = (uint8_t *)&retw, *inw8 = (uint8_t *)&inw;

	UCB0TXBUF = inw8[1];
	while ( !(UCB0IFG & UCRXIFG) )
		;
	retw8[1] = UCB0RXBUF;
	UCB0TXBUF = inw8[0];
	while ( !(UCB0IFG & UCRXIFG) )
		;
	retw8[0] = UCB0RXBUF;
	return retw;
}

3) UART output to console

4) Schematic:

Could you please help why SPI is not working?

Best regards,

Onur

**Attention** This is a public forum