This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5659: Driver Installation Issue

Part Number: MSP430F5659

Hi TI team,

We are trying to install msp430 Driver using command prompt.  We kept all the  required files in the same folder( .cat, .inf ,.xml). We followed the below command.

                                     pnputil -i -a msp430_ti_signed.inf

 It is working fine  and It is getting successfully installed in one PC. 

 

Problem:

I tried with another PC , then if I executed this command it shows access denied. Please advice on this issue on high priority

Regards

Manoj

  • Hi Manoj,

    Is this issue somehow related to your other thread from February 8th? If so, I can merge the two threads.
    Anyhow, when trying to install on the other PC, do you use a different OS or are you trying to install in a different location, possibly a location you don't have access rights to?

    Are you able to give more details on the error message you get in the command prompt when the installation fails?

    Thanks and best regards,
    Britta
  • Try running the command with a command prompt running as Administrator.
  • Hi TI team,

    Thanks for your response
    The Driver is working fine for windows 7 64 bit machine.

    The Driver installation setup for windows 7 64 bit machine is below
    The Installation folder contains(.cat, .inf ,.bat) then we run the batch as administrator.
    Batch file contain the commands pnputil -i -a c:\Driver\msp430_ti_signed.inf

    The Driver is not working for the windows 7 32 bit machine with the same setup.

    Please advice on this issue

    Regards
    Manoj
  • Hi TI team,

    Thanks for your response
    The Driver is working fine for windows 7 64 bit machine.

    The Driver installation setup for windows 7 64 bit machine is below
    The Installation folder contains(.cat, .inf ,.bat) then we run the batch as administrator.
    Batch file contain the commands pnputil -i -a c:\Driver\msp430_ti_signed.inf

    The Driver is not working for the windows 7 32 bit machine with the same setup and error we are getting is" windows encountered an error while installing driver for your computer"
    Is this inf file common for 64 bit and 32 bit machine or it is only for 64 bit machine?

    Please advice on this issue

    Regards
    Manoj
  • Hi Manoj,

    the inf file should support both 32 Bit and 64 Bit.

    To check if the inf file is working you could try to conduct the installation right clicking on the device in the device manager. Even though this is not the way you want to install the driver this could at least rule out that there's no general problem with the inf file you use.

    If you want to install the drivers on a WIN32 machine, did you check if you use the correct DPInst.exe for 32 Bit and not 64 Bit?

    Best regards,

    Britta

  • Hi Manoj,

    I intend to close this thread as I didn't here from you anymore. Were you able to solve your issue and move on with your application?

    Please feel free to comment again if you look for further assistance, I will then re-open the thread.

    Best regards,
    Britta
  • Hi britta,
    Thanks for your support!

    The Driver is working fine in both 32 bit also. We tried in PC in which driver is not installed before. Then it worked fine
    Please close this issue

    Thanks and Regards
    Manoj
  • Hi Manoj,

    glad to hear that it works just fine now.
    Could you please check the "Verify answer"?

    I'll close the thread then.

    Thanks and best regards,
    Britta

**Attention** This is a public forum