Hi TI Experts,
Please let me confirm the following question.
[Question]
Is there a possibility that MSP430 will be broken if erased the the TLV structure in Segment A on Flash?
Best regards.
Kaka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kaka,
Please see my comments in the related thread below.

Regards,
James
MSP Customer Applications
Why do you say "msp430 broken"? While you were testing - it was running original firmware, right? Maybe firmware is breaking msp430?
To determine that "msp430 is broken", it must be flashed with simple test code like LED flasher that runs on default DCO settings. If such code fail to operate correctly, then we can suspect that something happened to msp430.
In short: By erasing calibration data segment, you can break only firmware that depends on calibration values, not msp430 itself.
Further reading: my post in the other thread.
**Attention** This is a public forum