Part Number: MSP430F427
Other Parts Discussed in Thread: MSP-FET
Hi,
I'm trying to flash MSP430F427 from commands line via JTAG and at the end I've got Exit 16 and Error: unknown device.
Do I use wrong arguments or it's flasher bug? (by the way, CCS6,IAR flashing works just fine).
Full log:
HOME: ~/MSPFlasher_1.3.16$ sudo ./MSP430Flasher -n MSP430F427 -w 1p_max_gp_210416.txt -m jtag -v -z [VCC]
* -----/|-------------------------------------------------------------------- *
* / |__ *
* /_ / MSP Flasher v1.3.16 *
* | / *
* -----|/-------------------------------------------------------------------- *
*
* Evaluating triggers...done
* Checking for available FET debuggers:
* Found USB FET @ ttyACM0 <- Selected
* Initializing interface @ ttyACM0...done
* Checking firmware compatibility:
* FET firmware is up to date.
* Reading FW version...done
* Setting VCC to 3000 mV...done
* Accessing device...
# Exit: 16
# ERROR: Unknown device
* Starting target code execution...done
* Disconnecting from device...done
*
* ----------------------------------------------------------------------------
* Driver : closed (Internal error)
* ----------------------------------------------------------------------------
Regards,
Ugra