Part Number: MSP430F1611
Other Parts Discussed in Thread: MSP430FR4133,
Dear all,
I am trying to interface TelosB with external device called smartmesh mote "www.linear.com/.../4330".
Here, the example they used for interfacing to the mote was MSP430fr4133 launch pad which is quite different from TelosB(msp430f1611).
Referring to the code, LCD functions are not concerned at initialising board can be done seperately with my existing code.
The part I am stuck in with is this part of code:
void fsm_scheduleEvent(uint16_t delay, fsm_timer_callback cb) {
// remember what function to call
app_vars.fsmCb = cb;
// configure/start the RTC
RTCCTL = 0;
RTCMOD = delay; // delay (in 32kHz clock cycles)
RTCCTL |= RTCIE; // enable interrupts
RTCCTL |= RTCPS_0; // divider /1
RTCCTL |= RTCSS_2; // clock source is XT1CLK
RTCCTL |= RTCSR; // reset the RTC
}
Please correct me if I am wrong, but as far as I know for MSP430f1611, there is no RTC library available.
Could anyone direct me how to go about with this?
full code is attached in this post.
Thank you
Kind regards
#include "board.h"
#include <stdint.h>
#include "dn_ipmt.h"
//=========================== defines =========================================
// mote state
#define MOTE_STATE_IDLE 0x01
#define MOTE_STATE_SEARCHING 0x02
#define MOTE_STATE_NEGOCIATING 0x03
#define MOTE_STATE_CONNECTED 0x04
#define MOTE_STATE_OPERATIONAL 0x05
// service types
#define SERVICE_TYPE_BW 0x00
// timings
#define SERIAL_RESPONSE_TIMEOUT 16384 // 16384@32kHz = 500ms
#define CMD_PERIOD 32768 // 32768@32kHz = 1s
#define ONE_SEC 32768 // 32768@32kHz = 1s
#define DATA_PERIOD_S 10 // number of second between data packets
// app
#define NUM_STEPS 8
#define DIRECTION_UP 1
#define DIRECTION_DOWN 0
// api
#define SRC_PORT 0xf0b8
#define DST_PORT 0xf0b8
//=========================== typedef =========================================
typedef void (*fsm_timer_callback)(void);
typedef void (*fsm_reply_callback)(void);
//=========================== variables =======================================
typedef struct {
// fsm
fsm_timer_callback fsmCb;
// reply
fsm_reply_callback replyCb;
// app
uint8_t counter;
uint8_t secUntilTx;
uint8_t direction;
// api
uint8_t socketId; // ID of the mote's UDP socket
uint8_t replyBuf[MAX_FRAME_LENGTH]; // holds notifications from ipmt
uint8_t notifBuf[MAX_FRAME_LENGTH]; // notifications buffer internal to ipmt
} app_vars_t;
app_vars_t app_vars;
//=========================== prototypes ======================================
// fsm
void fsm_scheduleEvent(uint16_t delay, fsm_timer_callback cb);
void fsm_cancelEvent(void);
void fsm_setCallback(fsm_reply_callback cb);
// ipmt
void dn_ipmt_notif_cb(uint8_t cmdId, uint8_t subCmdId);
void dn_ipmt_reply_cb(uint8_t cmdId);
// app
uint16_t nextValue(void);
// api
void api_response_timeout(void);
void api_getMoteStatus(void);
void api_getMoteStatus_reply(void);
void api_openSocket(void);
void api_openSocket_reply(void);
void api_bindSocket(void);
void api_bindSocket_reply(void);
void api_join(void);
void api_join_reply(void);
void api_sendTo(void);
void api_sendTo_reply(void);
//=========================== main ============================================
int main(void) {
// hold the watchdog timer
WDTCTL = WDTPW + WDTHOLD;
// initialize board
board_init();
// reset local variables
memset(&app_vars,0,sizeof(app_vars));
// initialize the ipmt module
dn_ipmt_init(
dn_ipmt_notif_cb, // notifCb
app_vars.notifBuf, // notifBuf
sizeof(app_vars.notifBuf), // notifBufLen
dn_ipmt_reply_cb // replyCb
);
// schedule the first event
fsm_scheduleEvent(CMD_PERIOD, &api_getMoteStatus);
__bis_SR_register(LPM0_bits | GIE);
}
//=========================== private =========================================
//===== fsm
void fsm_scheduleEvent(uint16_t delay, fsm_timer_callback cb) {
// remember what function to call
app_vars.fsmCb = cb;
// configure/start the RTC
RTCCTL = 0;
RTCMOD = delay; // delay (in 32kHz clock cycles)
RTCCTL |= RTCIE; // enable interrupts
RTCCTL |= RTCPS_0; // divider /1
RTCCTL |= RTCSS_2; // clock source is XT1CLK
RTCCTL |= RTCSR; // reset the RTC
}
void fsm_cancelEvent(void) {
// stop the RTC
RTCCTL = 0;
// clear function to call
app_vars.fsmCb = NULL;
}
void fsm_setCallback(fsm_reply_callback cb) {
app_vars.replyCb = cb;
}
//===== ipmt
void dn_ipmt_notif_cb(uint8_t cmdId, uint8_t subCmdId) {
dn_ipmt_events_nt* dn_ipmt_events_notif;
switch (cmdId) {
case CMDID_EVENTS:
// parse notification
dn_ipmt_events_notif = (dn_ipmt_events_nt*)app_vars.notifBuf;
switch (dn_ipmt_events_notif->state) {
case MOTE_STATE_IDLE:
fsm_scheduleEvent(CMD_PERIOD,api_getMoteStatus);
break;
case MOTE_STATE_OPERATIONAL:
fsm_scheduleEvent(CMD_PERIOD,api_sendTo);
break;
default:
// nothing to do
break;
}
break;
default:
// nothing to do
break;
}
}
void dn_ipmt_reply_cb(uint8_t cmdId) {
app_vars.replyCb();
}
//===== app
uint16_t nextValue(void) {
uint16_t newValue;
// decide whether to go up or down
if (app_vars.counter==0) {
app_vars.direction = DIRECTION_UP;
}
if (app_vars.counter==NUM_STEPS-1) {
app_vars.direction = DIRECTION_DOWN;
}
// calculate new value
if (app_vars.direction==DIRECTION_UP) {
app_vars.counter++;
} else {
app_vars.counter--;
}
newValue = 0x10000/NUM_STEPS;
newValue *= app_vars.counter;
return newValue;
}
//===== api
void api_response_timeout(void) {
// issue cancel command
dn_ipmt_cancelTx();
// schedule first event
fsm_scheduleEvent(CMD_PERIOD, &api_getMoteStatus);
}
//=== getMoteStatus
void api_getMoteStatus(void) {
// arm callback
fsm_setCallback(api_getMoteStatus_reply);
// issue function
dn_ipmt_getParameter_moteStatus(
(dn_ipmt_getParameter_moteStatus_rpt*)(app_vars.replyBuf)
);
// schedule timeout event
fsm_scheduleEvent(SERIAL_RESPONSE_TIMEOUT, api_response_timeout);
}
void api_getMoteStatus_reply(void) {
dn_ipmt_getParameter_moteStatus_rpt* reply;
// cancel timeout
fsm_cancelEvent();
// parse reply
reply = (dn_ipmt_getParameter_moteStatus_rpt*)app_vars.replyBuf;
// choose next step
switch (reply->state) {
case MOTE_STATE_IDLE:
fsm_scheduleEvent(CMD_PERIOD, &api_openSocket);
break;
case MOTE_STATE_OPERATIONAL:
fsm_scheduleEvent(CMD_PERIOD,api_sendTo);
break;
default:
fsm_scheduleEvent(CMD_PERIOD, api_getMoteStatus);
break;
}
}
//=== openSocket
void api_openSocket(void) {
// arm callback
fsm_setCallback(api_openSocket_reply);
// issue function
dn_ipmt_openSocket(
0, // protocol
(dn_ipmt_openSocket_rpt*)(app_vars.replyBuf) // reply
);
// schedule timeout event
fsm_scheduleEvent(SERIAL_RESPONSE_TIMEOUT, api_response_timeout);
}
void api_openSocket_reply(void) {
dn_ipmt_openSocket_rpt* reply;
// cancel timeout
fsm_cancelEvent();
// parse reply
reply = (dn_ipmt_openSocket_rpt*)app_vars.replyBuf;
// store the socketID
app_vars.socketId = reply->socketId;
// choose next step
fsm_scheduleEvent(CMD_PERIOD, api_bindSocket);
}
//===== bindSocket
void api_bindSocket(void) {
// arm callback
fsm_setCallback(api_bindSocket_reply);
// issue function
dn_ipmt_bindSocket(
app_vars.socketId, // socketId
SRC_PORT, // port
(dn_ipmt_bindSocket_rpt*)(app_vars.replyBuf) // reply
);
// schedule timeout event
fsm_scheduleEvent(SERIAL_RESPONSE_TIMEOUT, api_response_timeout);
}
void api_bindSocket_reply(void) {
// cancel timeout
fsm_cancelEvent();
// choose next step
fsm_scheduleEvent(CMD_PERIOD, api_join);
}
//===== join
void api_join(void) {
// arm callback
fsm_setCallback(api_join_reply);
// issue function
dn_ipmt_join(
(dn_ipmt_join_rpt*)(app_vars.replyBuf) // reply
);
// schedule timeout event
fsm_scheduleEvent(SERIAL_RESPONSE_TIMEOUT, api_response_timeout);
}
void api_join_reply(void) {
// cancel timeout
fsm_cancelEvent();
// choose next step
// no next step at this point. FSM will advance when we received a "joined"
// notification
}
//===== sendTo
void api_sendTo(void) {
uint8_t payload[2];
uint8_t dest_addr[16];
// send only every DATA_PERIOD_S seconds
if (app_vars.secUntilTx>0) {
// decrement number of second to still wait
app_vars.secUntilTx--;
// cancel timeout
fsm_cancelEvent();
// choose next step
fsm_scheduleEvent(ONE_SEC, api_sendTo);
return;
} else {
app_vars.secUntilTx = DATA_PERIOD_S;
}
// arm callback
fsm_setCallback(api_sendTo_reply);
// create payload
dn_write_uint16_t(payload, nextValue());
memcpy(dest_addr,ipv6Addr_manager,16);
// issue function
dn_ipmt_sendTo(
app_vars.socketId, // socketId
dest_addr, // destIP
DST_PORT, // destPort
SERVICE_TYPE_BW, // serviceType
0, // priority
0xffff, // packetId
payload, // payload
sizeof(payload), // payloadLen
(dn_ipmt_sendTo_rpt*)(app_vars.replyBuf) // reply
);
// schedule timeout event
fsm_scheduleEvent(SERIAL_RESPONSE_TIMEOUT, api_response_timeout);
}
void api_sendTo_reply(void) {
// cancel timeout
fsm_cancelEvent();
// choose next step
fsm_scheduleEvent(ONE_SEC, api_sendTo);
}
//=========================== interrupts ======================================
#pragma vector = RTC_VECTOR
__interrupt void RTC_ISR(void) {
volatile uint16_t iv;
iv = RTCIV;
app_vars.fsmCb();
}