Part Number: MSP430G2553
Hi
I was trying to post my question in this thread, however, it is locked!
I am connecting the MSP430G2553 to the ADXL345 accelerometer over SPI and using this code to set the ADXL345:
///////////////////////////////////////////////////////////////////
void SPI_write(void){
P3OUT &= ~CS; // BIT 3.7 is CS
while (!(IFG2&UCA0TXIFG)); // Wait for TXBUF ready
UCA0TXBUF = 0x2D; // We want to write to the power register
while (!(IFG2&UCA0TXIFG)); // Wait for TXBUF ready
UCA0TXBUF = 0x00; // Write the 0x00 to the power register (put the ADXL345 in standby mode)
///--------------------------------------------------------
while (!(IFG2&UCA0TXIFG)); // Wait for TXBUF ready
UCA0TXBUF = 0x31; // We want to write to the data format register while the ADXL345 is in stanby mode
while (!(IFG2&UCA0TXIFG)); // Wait for TXBUF ready
UCA0TXBUF = 0x09; // Write the 0x01 to the data format register (4g range)
///--------------------------------------------------------
while (!(IFG2&UCA0TXIFG)); // Wait for TXBUF ready
UCA0TXBUF = 0x2C; // We want to write to the BW_RATE register
while (!(IFG2&UCA0TXIFG)); // Wait for TXBUF ready
UCA0TXBUF = 0x09; // Write 0x09 to the BW_RATE register to set the ACC to 25Hz data rate (table 7, p#14 of datasheet)
// setting the ACC to this acceleration sampling rate should makes it consume 90microAmp.
//see note 7 on page 5 of the data sheet about the wake up time
///---------------------------------------------------------
while (!(IFG2&UCA0TXIFG)); // Wait for TXBUF ready
UCA0TXBUF = 0x2D; // We want to write to the power register
while (!(IFG2&UCA0TXIFG)); // Wait for TXBUF ready
UCA0TXBUF = 0x08; // Write the 0x08 to the power register to put it in measure mode
///---------------------------------------------------------
delay_ms(10);
while (!(UCB0STAT&UCBUSY)==0);
IFG2 &= ~UCA0RXIFG;
P3OUT |= CS;
}
////////////////////////////////////////////////////////////////////////
I am getting back the data. But it is different from when the ADXL345 is connected to the Arduino.
For example, when he accelerometer is still on the table, then I get 0.79 G rather than 1 G for the z-axis
anyone can help me with this
thank you