This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2418: Will MSP430 get damaged if pin 1.2 is pulled down to 2V?

Part Number: MSP430F2418


Team,

Can you help address customer's question below:

I am investigating an issue with a component on one of our PCBs.

The component is connected to a micro pin that is set to output high but the attached component has failed and results in a load of 20 Ohms on the Pin.

Processor:                                           MSP430F2418

Pin:                                                        P1.2

VCC:                                                      3.2 Volts

Attached Component:                   Piezo Buzzer

The Pin is pulled down to 2 Volts as a result.  The question is if the failed component is replaced what is the expected damage to the microcontroller pin.

I understand that the micro will not function properly while the load is present but will it damage it beyond functioning.

Thanks

Viktorija

**Attention** This is a public forum