This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1002: Flow detection limitation

Part Number: TIDM-1002

Dear Champs,

I notice in sec 3.2.2.3 in the doc (), it says the minimum flow detection is 7.95 lph, calculated under the maximum flow of 4930lph.

Is "the maximum flow of 4930lph" the limitation of the max flow that can be detected or is it just used in the case?

That is, if our customer wants to use this design for larger flow, 12000 to 90000 lph, can it be used?

Or what should they modify?

Also, besides FR5994, we also have FR6047.

Will there be gas meter on FR6047?

If yes, when is it available and what will be the major difference? Say, more accuracy?

**Attention** This is a public forum