This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2132: Develop Firmware MSP430

Part Number: MSP430F2132


I'm having another challenge so you can help me and develop together if possible. I hope you can help me to succeed again in this and in the next. I want to post in Forúm also to get a certain score. The following is a descriptive and attached diagram.
Develop a firmware to control a hardware composed of an MSP430F2132 microcontroller, a rectifier bridge, an optocoupler and an LED. A P1 port pin should be configured as a digital input associated with external interrupt. The red LED should change state every 20 grid periods.

Thank you.

  • Hi,

    The best way to utilize the MSP Low-Power Microcontroller forum is to post more direct questions about an issue or idea you're working on . This is not a space to ask homework questions.

    If you've attempted to solve this problem yourself, let us know what you've tried and what you're having difficulty with. We're more than happy to point you to helpful code examples, review  your code, and explain the subtleties of designing an MSP430 into your system.

    When starting design with an MSP430, I always recommend reading the devices User's Guide, Datasheet, and the exploring relevant code examples. Try this approach and let me know if you have any specific questions I can help you with.

    Best regards,

    Caleb Overbay

**Attention** This is a public forum