This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/MSP432P401R: Runtime Object Viewer Enhancements (historical logs)

Part Number: MSP432P401R

Tool/software: TI-RTOS

Hey,

I've just recently realised that the new ROV is a lot more capable than the old one, so I've begun having a play with it and I'm really liking it. Works better, nice graphs, etc. etc. I'm especially liking the repeated refresh functionality because it allows us to capture data over time. The Heap Free Space and CPU Load graphs are particularly helpful, so I'm wondering if this can be extended to normal modules and not just Add Ons. For example, I use logs extensively, but only have limited memory on the device for buffering, so I can see the most recent 30 or so messages. But with repeated refreshing, we can dump data from the device relatively quickly, so I should be able to clear my log buffer before it completely changes. However, as far as I can tell, the current view for LoggerMin only shows the data that is stored on the device. Is it possible to display a history of the logs, so I can see a lot more of what as happened? i.e. logs 0 - n, instead of just what's in the buffer?

Cheers

Campbell

**Attention** This is a public forum