Other Parts Discussed in Thread: ENERGIA
Hello there,
I have read on other threads there is a problem with MSP430G2 launchpad board drivers with Windows 10, the problem I have is unstable USB-to-UART driver operation, it works and stops randomly. While the debugging/programming feature works fine, I can still program and debug the LP, but using the USB-to-UART is quite bothersome because of this issue, so far I have tried all TUSB4310 drivers from TI and MSP430G2 LP drivers from Energia with no luck. I tried to disable driver signature enforcement in Windows 10 but no luck either, still the USB-to-UART works randomly. On one of the threads on the e2e forum it was mentioned to wait for some time (3-10 seconds) before communicating with the board, I tried that as well without any luck.
Any more suggestions on the matter?. (Board rev.: 1.5, OS: Windows 10 x64)
Cheers,
Karim