Hi,
I'm having the following problem:
Communication error.
Check if hardware is connected.
Check if debug protocol (SBW or 4-wire) is correct.
This error appears when Download and debug in IAR Embedded Workbench. In CCS v4, the archive msp430f5529.ccxml has invalid character.
I checked all jumpers and are configured for 4-wire JTAG. Jumpers JP5, JP6, JP7, JP8, JP9, JP10 are connect to pins 2 and 3. The board is supplied for MSP-FET430UIF. JP3 is connect to pins 1 and 2, and JP4 is not connect.
Regards,
JFK