I just recently purchased this product for my project and had read the user guide available in the CD
1. can someone offer help such as additional references or documents with regards to usage of product?
2. which i/o pin(of the mcu) can i use to connect to a external temperature sensor?
3. is it okay for me to configure the pins, or are the settings fixed?
4. is there a way to obtain data only from an external temperature sensor besides taking from the built in sensor?
Thanks in advance