Other Parts Discussed in Thread: CC3220SF-LAUNCHXL
Namaste Support Executive,
We've recently purchased the MSP430-F6736 EVM Kit for E-metering. For software, I've downloaded the IAR Embedded Workbench v7.11 (Kickstarter 8k code limited). Details are as below.
When I double click and attempt to open the ..\slaa517e\slaa517\SLAA517\Source\emeter-ng\emeter.eww, I'm prompted for a conversion twice, to which I agree. However, the IAR Workbench crashes and prompts me to send the error dump before auto closing. Details are as below.
The ZIP of the Crash dump is additionally enclosed below.
83876ac0-84f5-4b5c-a683-6eb84b04b227.zip
My questions:
1. I'm unable to find the emeter-6736.epw project in the slaa517 folder. Everything is specific to 6733. Is the same code valid for evm6736 kit? The slaa517e PDF under Section 5.2.1 reads as below -
"The folder "emeter-ng" contains multiple project files. For this application, the emeter-6736.ewp project file is to be used. The folder "emeter-toolkit" has corresponding project file emeter-toolkit-6736.ewp. Choose only the projects that have the succeeding terms 6736 for this application. For first time use, it is recommended that both the projects be completely rebuild."
2. How do I resolve this issue to open the emeter.eww workspace?
3. How do I migrate the code to TI's Code Composite Studio? What is the recommended version of this IDE for building the existing sample code?
Thanks | Regards,
Dipen Shah