Part Number: MSP432E401Y
Hello, I have been referencing the Launchpad schematic for this device, which has an embedded USB debugger on it. I am looking for the simplest programming method possible, but it looks like there are several 10,14, 20 pin pinouts for different JTAG ports. I don't want to have to use any kind of adapter for my programming header, so which of these pinouts should I use for the most standard programmer? I am coming from more of an Microchip ATmega background, where I can use a simple ISP programmer to flash my device, and it's a standard 6 pin pinout.
What should I use for a connector and pinout to not limit my programming options later?