Hi Experts,
I previously used the same resonator as the 5529LP in my 5528 design and was able to leverage USB BSL programming in my factory flow. That resonator is Murata's CSTCR4M00G15L99-R0 which is not REACH compliant. I migrated my latest design to AVX's PBRV4.00MR50Y000 which is a REACH compliant alternative. When I received my first prototypes with this new resonator, the board was not recognized in USB BSL mode. I flashed the board using SBW, and the USB functionality worked as normal. Later, I took one of the prototypes, and replaced its AVX resonator with the old Murata resonator. I didn't expect this to be a problem, but it turns out that board now works in USB BSL mode with the Murata resonator.
Can you explain why USB BSL will work with one 4MHz resonator but not with the other? Keep in mind the board works with both resonators after it has been flashed.
Do you have recommendation for REACH compliant resonator that will work with USB BSL?
Thanks,
Ren