Part Number: MSP430F6736
Other Parts Discussed in Thread: , MSP-FET
Hi all,
I am using the MSP430F6736. It is a very interesting device. I have done some measurements as testing and i know how to use the device. I had some problems with IAR's version, but they are solved and i can programming the device (I have tested that it is correct). At this momment i am reprogramming the MSP430F6736 because i have the academic objective (i am a Master's student, thi) of doing a similar system but much more simply. I pretend only doing measures of current, voltage, active power, reactive power and energies, power factor and frequency for a single phase. The process that i have followed for understanding the code is reading the coments of the slaa517 files (.c and .h, both extension files), seaching the functions in Internet and IAR software, looking the MSP430F6736A datasheet (www.ti.com/.../msp430f6736a.pdf) and the EVM430F6736 datasheet (www.ti.com/.../slaa517e.pdf).
I began modifying the code of the emeter-foreground.c device (I am reprogramming throught the slaa517 file). The changes that i have done are ok, becausei have used the MSP-FET(http://www.ti.com/tool/MSP-FET) , but i have some doubts.
1. At this momment i am not sure of where are the definitions of the meter which are used in the extension files .c (the definitions are in emeter.h, emeter-toolkit.h, emeter-structs.h, emeter 1-phase.h). I want to say that in the code is common say, for example, "#if defined(MAINS_FREQUENCY_SUPPORT)" , and there are libraries where it iappears "define MAINS_FREQUENCY_SUPPORT". My question about the previous is in which of those are? (emeter.h or emeter 1-phase.h, i supose).
2. There are some variables that i don't understand very good (and i am not sure if they have been used in the EVM430F6736, this doubt is in part interconected with doubdt 1).
2.1. I know the variable PHASE_CORRECTION_SUPPORT is used because you have a CT in the EVM device, but DYNAMIC_PHASE_CORRECTION_SUPPORT? I think it doesn't had to be used in this case, but i am not sure and i dont understand very well the explanation.
2.2. LIMP_MODE_SUPPORT. I don't understand the cases in that it could be used. I don't know if it is used in this device.
2.3. NEUTRAL_MONITOR_SUPPORT. It is explained in the emeter.h that "This switch enables monitoring of the neutral lead for anti-fraud purposes.". I don´t understand very good that and if it is necessary that variable for my case
2.4. PER_SENSOR_PRECALCULATED_PARAMETER_SUPPORT. I don't know nothing about that variable because it is not defined in the libraries.
At this moment i have that doubts and i pretend solving that before going to next step (modify emeter-background.c). Can someone help me?
Thanks in advance