Part Number: MSP430F4794
Dear Sirs:
Could I get MSP430F4794 thermal parameter such as RθJA RθJC and so on. We check no this parameter in datasheet, we demand the part can work at 45°C or higher, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F4794
Dear Sirs:
Could I get MSP430F4794 thermal parameter such as RθJA RθJC and so on. We check no this parameter in datasheet, we demand the part can work at 45°C or higher, thanks.
Hi,
the part is specified to work between -40°C and 85°C.
Please have a look in data sheet on page 24, table recommended operating conditions, parameter: Operating free-air temperature range. http://www.ti.com/lit/slas545
Best regards,
Andre
**Attention** This is a public forum