This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2633: UART Bluetooth

Part Number: MSP430FR2633

Hello,

I am working with " MSP-CAPT-FR2633 Development kit ", and for a portable project, I need to connect the 

setup to the Bluetooth module. My question is that, can I connect the controller directly to the bluetooth module (such as HC-05)

with UART pins and receive the value on the PC.

I would appreciate if you help me.

Thank you

  • Hello Narges,
    yes, if your question applies to whether the MSP430FR2633 is able to support the UART communication with the HC-05 Bluetooth module.
    Please look at this post in the CC26xx related forum, where you can find useful information about the UART communication with the HC-05. The displayed code is not for the MSP430FR2633, but it easily could be adopted to the UART module of the MSP430 device.
    e2e.ti.com/.../2447489

    Best regards
    Peter

**Attention** This is a public forum