This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Software Algorithm equivalent for hardware CRC16

Part Number: MSP432P401R
Other Parts Discussed in Thread: MSP430F5529

Hi,

I am looking for code that implements the CRC16 calculation the way the peripheral does on the MSP432. It does not appear to be what I’ve used for the MSP430 for many years, and it’s not detailed in the MSP432 DriverLib User’s Guide.

I was able to find the hardware schematic in the MSP432 Users Guide/Technical Reference Manual (SLAU356H) but am still unclear what software algorithm would be equivalent to this hardware.

 Any thought on where to look?

Thanks!  Blake

  • Blake,
    If you look at this example the HW result is compared with the software result, where the software implementation is provided in the function call.

    dev.ti.com/.../

    Something simple to check is to compare with the CRC example for MSP430. The example currently available does not do the bit reversal but the APIs are available to do an apples-to-apples comparison. I will try and make that comparison and get back to you.

    Chris
  • Blake,

         I did a quick test and confirm that the result is the same.  Please find the attached MSP430F5529 example updated to match the MSP432 example mentioned in the previous post.  

    /* --COPYRIGHT--,BSD
     * Copyright (c) 2017, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     * --/COPYRIGHT--*/
    //******************************************************************************
    //!
    //! CRC - Build Signature and Rebuild to test.
    //!
    //!  The CRC is first used to build a signature using a seed and multiple data
    //!  values. This signature is considered as the checksum and can be sent by a
    //!  UART connection along with the data to verify the correct data has been
    //!  sent. The second half of this program is used to test the CRC checksum of
    //!  the data that has been created, by recreating the same checksum and
    //!  comparing it to the first checksum. If the two checksum are equal, then
    //!  P1.0 is set and the LED is turned on. Breakpoints can be set before the
    //!  CRC_setData() function to observe the CRC register values and see the
    //!  subsequent signatures before/after each data set.
    //!
    //!  Tested On: MSP430F5529,MSP430FR5739
    //!             -----------------
    //!         /|\|                 |
    //!          | |                 |
    //!          --|RST              |
    //!            |             P1.0|--> LED
    //!            |                 |
    //!
    //!
    //! This example uses the following peripherals and I/O signals.  You must
    //! review these and change as needed for your own board:
    //! - CRC peripheral
    //! - GPIO Port peripheral
    //!
    //! This example uses the following interrupt handlers.  To use this example
    //! in your own application you must add these interrupt handlers to your
    //! vector table.
    //! - NONE
    //!
    //******************************************************************************
    
    #include "driverlib.h"
    
    void main (void)
    {
        //uint16_t crcSeed = 0xBEEF;
        uint16_t crcSeed = 0xFFFF;
    //    uint16_t data[] = {0x0123,
    //                           0x4567,
    //                           0x8910,
    //                           0x1112,
    //                           0x1314};
        uint8_t data[] = {0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39};
        uint16_t crcResult;
        uint8_t i;
    
        //Stop WDT
        WDT_A_hold(WDT_A_BASE);
    
        //Set P1.0 as an output
        GPIO_setAsOutputPin(
            GPIO_PORT_P1,
            GPIO_PIN0);
    
        //Set the CRC seed
        CRC_setSeed(CRC_BASE,
            crcSeed);
    
    //    for (i = 0; i < 5; i++)
        for (i = 0; i < 9; i++)
        {
            //Add all of the values into the CRC signature
    //        CRC_set16BitData(CRC_BASE,
    //            data[i]);
            /*
             * similar to 432 example
             */
            CRC_set8BitDataReversed(CRC_BASE,data[i]);
    
        }
    
    
        //Save the current CRC signature checksum to be compared for later
        crcResult = CRC_getResult(CRC_BASE);
    
    
        //*** Test the CRC ***//
    
        //Reset the CRC Signature and set the same seed
        CRC_setSeed(CRC_BASE,
            crcSeed);
    
    //    for (i = 0; i < 5; i++)
        for (i = 0; i < 9; i++)
        {
            //Add all of the values into the CRC signature
    //        CRC_set16BitData(CRC_BASE,
    //            data[i]);
            /*
             * similar to 432 example
             */
            CRC_set8BitDataReversed(CRC_BASE,data[i]);
        }
    
        //Compare the 2 CRC Resulting Signature Checksums
        if (crcResult == CRC_getResult(CRC_BASE)){
            //set P1.0
            GPIO_setOutputHighOnPin(
                GPIO_PORT_P1,
                GPIO_PIN0);
        }
    
        //Enter LPM4, interrupts enabled
        __bis_SR_register(LPM4_bits);
        __no_operation();
    }
    
    

    Regards,

    Chris

  • Thanks a bunch Chris!

**Attention** This is a public forum