This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP432E401Y: MSP-EXP432P401R

Part Number: MSP-EXP432E401Y


Is the MSP-EXP432P401R_Software Examples directly portable to the MSP-EXP432E401Y in the CCS

appart the EXP432P401R.cmd to MSP_EXP432E401.cmd  and board.h file  and the target config?

Thanks 

  • Denis,
    It depends on which set of examples you are looking at. The TI-RTOS-based (TI Drivers) examples from MSP432P401 can be dropped into the MSP432P4111 empty project with no changes and run directly.

    The driverlib and, particularly, the register-level examples will likely need changes due to differences in the underlying hardware architecture.
    Regards,
    Bob L.

**Attention** This is a public forum