This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2453: Internal clock source drift due to temperature change

Part Number: MSP430G2453

Seeing the internal clock drift with temperature - close to the +3% 0-85C specification.  Looking for a cost effective way to compensate drift. 

  • If there is need for precise clock source, than external one (XT crystal) should be used.

  • Is there any statistical data available from TI on typical temperature coefficient?  If there is could a software compensation algorithm be used to partially correct the clock based on temperature?

  • Hello Paul,

    The MSp430G2453 and the rest of the G series of MSP430s have calibrated DCO constants written into Info Memory for you to use. You have to use these constants to get the Datasheet numbers you saw. In our code examples for the part we do provide a routine to do your own calibration constants, which you could potentially do at different temps. That being said, even after calibration, these parts are getting around a 3% tolerance depending on the frequency being used. as zrno soli mentioned, if you need more accuracy in your clock, then a LF Xtal is recommended.

**Attention** This is a public forum