Part Number: MSP430FR2422
Hi,

RHL package, A5 is assigned on Pin 12.
But on below pin description table, A5 is assigned to Pin 10. Which one is right? Is it a writing mistake?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR2422
Hi,

RHL package, A5 is assigned on Pin 12.
But on below pin description table, A5 is assigned to Pin 10. Which one is right? Is it a writing mistake?
Hi Daniel,
you're right. The other parts of the table. related to the ADC pin assignments also does not cope with the package pin assignment. The package view is corresponding with the control bit table for the Pin Functions Table 6-16 Port 2, and it also makes sense from the sequence of the ADC pins going clockwise from A0-A7.
Please see the table 6-16 here below.
You could verify that, by testing the bits and applying signals to the ADC input. We will check the datasheet, and try to update as soon as possible. Many thanks for the feedback.
Best regards
Peter
**Attention** This is a public forum