This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR4133: multiple ADC channel sequencing reading probblem

Part Number: MSP430FR4133

Hello ,

 I am working on MSP430FR4133 launch pad"s ADC. i have trying to read single channel its working fine with ADC channel A8 but when i am tried to work with sequential A7 and A8 using Sequence-of-channels and Repeat-sequence-of-channels mode using ADCSC bit as ADC sample-and-hold source its not working.i am giving constant 0.50 Vdc to pin no P8.0 And P1.7 which are A8 and A7 respectively are giving random value which i have pasted in image.as i am expecting around 342 decimal count because ref is 1.5V internal and 10 bit ADC.

circuit configurations are ground is shorted and common 0.5V is directly fed to the ADC channel through voltage divider and a low pass RC filter which value is 100 ohms and 2.2uF cap.

one more thing i have tried is that i had make one voltage divider array which out put is varies between 0 to 1.25V with step of 125mV using 10 step rotary switch.with this configuration i have use single channel and i am getting step of 84~85 decimal count when i am switching rotary switch which is exactly right but same configuration will not work for multiple channel.

my code is follow

 

#include <msp430.h>

int ADC_Result[2]; //10bit ADC conversion result array
unsigned char i;

int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT

// Configure ADC A7~8 pins
SYSCFG2 |= ADCPCTL8 | ADCPCTL7 ;

// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;

// Configure ADC
ADCCTL0 |= ADCSHT_2 | ADCMSC | ADCON; // 16ADCclks, MSC, ADC ON
ADCCTL1 |= ADCSHP | ADCCONSEQ_1; // ADC clock MODCLK, sampling timer, s/w trig.,single sequence
ADCCTL2 |= ADCRES; //10bit conversion results
ADCMCTL0 |= ADCINCH_8 | ADCSREF_1; // A7~8(EoS); Vref=1.5V
ADCIE |= ADCIE0; // Enable ADC conv complete interrupt

// Configure reference
PMMCTL0_H = PMMPW_H; // Unlock the PMM registers
PMMCTL2 |= INTREFEN; // Enable internal reference
__delay_cycles(400); // Delay for reference settling
__no_operation();

while(1)
{
i = 1;
while(ADCCTL1 & ADCBUSY); // Wait if ADC core is active
ADCCTL0 |= ADCENC | ADCSC; // Sampling and conversion start
__bis_SR_register(GIE);
__no_operation(); // Only for debugger
__delay_cycles(5000);
__no_operation();
}
}

// ADC interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC_VECTOR
__interrupt void ADC_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC_VECTOR))) ADC_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(ADCIV,ADCIV_ADCIFG))
{
case ADCIV_NONE:
break;
case ADCIV_ADCOVIFG:
break;
case ADCIV_ADCTOVIFG:
break;
case ADCIV_ADCHIIFG:
break;
case ADCIV_ADCLOIFG:
break;
case ADCIV_ADCINIFG:
break;
case ADCIV_ADCIFG:
ADC_Result[i] = ADCMEM0;
if(i == 0)
{

}
else
{
i--;
}
ADCIFG = 0;
break;
default:
break;
}
}

this is the same code which are present in sample code only change is that i have changed ADC channel and remove LPM mode

  • Hi Ajay
    could you please help to test FR4133 code example "msp430fr413x_adc10_10.c" firstly?
    Go trough the code provided, I think the problem is (from UG) "A sequence of channels is sampled and converted once. The sequence begins with the channel selected by the ADCINCHx bits and decrements to channel A0. Each ADC result is written to ADCMEM0. The sequence stops after conversion of channel A0".
  • CONSEQ=1 (or =3) with MSC=1 is a challenge on the FR2/4 since there's only one result word and no DMA.

    SLAU445G Figure 20-11 shows that with SHT=2 (16-clock sampling) each conversion takes (16+12+1)=29 ADC clocks. You should budget at least 30 CPU clocks to get into/out of the ISR, plus whatever you want to do there (so make a guess at 50 CPU clocks). The MODCLK is running at about 5x the CPU clock, so each conversion runs in about 5 CPU clocks.

    Result: You will not succeed in grabbing the first sample before the second sample overwrites it. (Even with ADCCLK=SMCLK[1MHz] you won't succeed.) I'm not at all convinced that adc10_10 works properly either, though I haven't tried it.

    Perhaps the simplest fix is to use ACLK (REFOCLK=32kHz), though this is pretty slow.

    Alternatively, using SMCLK and ADCDIV=7 would give you (29*8)=232 CPU clocks to grab the sample, which should be enough if you're not doing anything else.

    Keep in mind that the ADC will keep counting down through channels 6-0, interrupting each time, which (at 232 CPU clocks each) will take a while.
  • I was curious, so I tried example msp430fr413x_adc10_10.c, and indeed it fails -- in that case the symptom was that it never got out of LPM since the interrupts overran each other and "i" never reached 0.

    For that example, using ADCSSEL_2 [SMCLK] with ADCDIV_1 [/2] was (just barely) adequate.
  • #include <msp430.h>

    int ADC_Result[2]; // 8-bit ADC conversion result array
    int i=1;
    int a=0;
    int main(void)
    {
    WDTCTL = WDTPW | WDTHOLD; // Stop WDT

    // Configure ADC A7~8 pins
    SYSCFG2 |= ADCPCTL7 | ADCPCTL8;

    // Configure XT1 oscillator
    P4SEL0 |= BIT1 | BIT2; // P4.2~P4.1: crystal pins

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings
    PM5CTL0 &= ~LOCKLPM5;

    FRCTL0 = FRCTLPW | NWAITS0; // Set number of FRAM waitstates to 0

    CSCTL4 = SELMS__DCOCLKDIV | SELA__XT1CLK; // Set ACLK = XT1; MCLK = SMCLK = DCO

    do
    {
    CSCTL7 &= ~(XT1OFFG | DCOFFG); // Clear XT1 and DCO fault flag
    SFRIFG1 &= ~OFIFG;
    }while (SFRIFG1 & OFIFG); // Test oscillator fault flag


    // Configure ADC
    ADCCTL0 |= ADCSHT_2 | ADCMSC | ADCON; // 16ADCclks, MSC, ADC ON
    ADCCTL1 |= ADCSHP | ADCCONSEQ_3|ADCSSEL_1; // ADC clock ACLK, sampling timer, s/w trig.,Repeat-sequence-of-channels
    ADCCTL2 |= ADCRES; // 10-bit conversion results
    ADCMCTL0 |= ADCINCH_8 | ADCSREF_1; // A7-8(EoS); Vref=1.5V
    ADCIE |= ADCIE0; // Enable ADC conv complete interrupt

    // Configure reference
    PMMCTL0_H = PMMPW_H; // Unlock the PMM registers
    PMMCTL2 |= INTREFEN; // Enable internal reference
    __delay_cycles(400); // Delay for reference settling
    __no_operation();

    while(ADCCTL1 & ADCBUSY); // Wait if ADC core is active
    ADCCTL0 |= ADCENC | ADCSC; // Sampling and conversion start
    __bis_SR_register(GIE);
    while(1)
    {
    a++;
    if(a==10000) //just for check
    a=0;
    }
    }

    // ADC interrupt service routine
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=ADC_VECTOR
    __interrupt void ADC_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(ADC_VECTOR))) ADC_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
    switch(__even_in_range(ADCIV,ADCIV_ADCIFG))
    {
    case ADCIV_NONE:
    break;
    case ADCIV_ADCOVIFG:
    break;
    case ADCIV_ADCTOVIFG:
    break;
    case ADCIV_ADCHIIFG:
    break;
    case ADCIV_ADCLOIFG:
    break;
    case ADCIV_ADCINIFG:
    break;
    case ADCIV_ADCIFG:
    ADC_Result[i] = ADCMEM0;
    if(i == 0)
    {
    i = 1;
    }
    else
    {
    i--;
    }
    ADCIFG = 0;
    break;
    default:
    break;
    }
    }


    i have check this with clock of ACLK whi 32KHz and give same result as like decimal equivalent count vary from 425,777,1023,764,722,719,764,612 ( which is any random value ) while i am expecting output count is around 342 decimal which is equivalent to 0.5V with reference of 1.5V .
  • Hello ,
    my circuit which is basically three resistor array network ( each network can generate 0 to 1.25V with the step of 125mV) with rotary switch which control out put voltage followed by a low pass filter with cut off frequency is around 725Hz (100 ohms and 2.2UF cap) for each network..
    this circuit i have tested with MSP432 launch pad (14 bit ADC) with 2 channel sequentially which give proper 1700 decimal step which is correspond to 125mV
    now same board with MSP430FR4133 which give the problem as i mention in previous replies.

    i have pasted two different code in my replies  

    first one is of single sequence with internal clock 5MHz

    and repeat sequence with ACLK of 32KHz

    are they correct like TI suggestion ? or not .if not then what should i do change in the code.

    does this MSP430FR4133 launchpad actually support multiple channel sequencing ? does anyone did this actually sequential channel  sampling on MSP430FR4133 launch pad ? if yes please suggest what changes i should to work in sequential sequences sampling.  

  • > Keep in mind that the ADC will keep counting down through channels 6-0, interrupting each time,
    Your indexing scheme is storing the results from channels 6-0 over the ones from 8-7. The simplest change here is probably to expand ADC_Result[] to 9 entries to store them all, then ignore the first 7.

    * does anyone did this actually sequential channel sampling on MSP430FR4133 launch pad ?
    Per my previous response: I did this just last night. I didn't use CONSEQ=3 since you asked about CONSEQ=1, but the principle is pretty much the same.

    Unsolicited:
    > ADCIFG = 0;
    I recommend that you not do this, since reading ADCMEM0 clears ADCIFG0. It may not be causing trouble now, but it will eventually.
  • still dont get any result for sequential sampling with Code provided by TI. but time being i am switching channel manually and getting reading of multiple channel ( because it s decrease the speed of output rate but my application is slow so i am fine with it.

    """* does anyone did this actually sequential channel sampling on MSP430FR4133 launch pad ?
    Per my previous response: I did this just last night. I didn't use CONSEQ=3 since you asked about CONSEQ=1, but the principle is pretty much the same.""
    dear bruce as you worked on sequential sampling and working fine for you then can you paste your code which your applications (controller)is working cause i have tried TI provided code " msp430fr413x_adc10_10.c" its not working as its and also i have made code by setting ADC register to my application for sequential sampling(without LPM mode) with help of user guild which also not working (i have pasted all code above)so if you have working code with you then paste it to check my code where i am doing mistake and what changes you did in example code. or you can send to me on my personal email id ""ajaykhedekar1234@gmail.com""if your comfortable.

  • I don't have my materials here, but I suppose that this:

    > For that example, using ADCSSEL_2 [SMCLK] with ADCDIV_1 [/2] was (just barely) adequate.

    [see also SLAU445G Table 20-4] means I changed line 89 of msp430fr413x_adc10_10.c [SLAC625E] from this:

    > ADCCTL1 |= ADCSHP | ADCCONSEQ_1; // ADC clock MODCLK, sampling timer, s/w trig.,single sequence

    to this:

    > ADCCTL1 |= ADCSHP | ADCCONSEQ_1|ADCSSEL_2|ADCDIV_1; // SMCLK/2, sampling timer, s/w trig.,single sequence

    Did you try something like this? How about the other changes I suggested?
  • Hi all
    Thanks for your comment and sorry to be late!
    You are correct that msp430fr413x_adc10_10.c can not work correctly. the cause is multiple sample-and-conversion setting by ADCMSC.ADCCTL0. interrupt handling of ADC spend longer time than ADC conversion. This cause that the ADC conversion result is not correctly handled in msp430fr413x_adc10_10.c code example.
    We will update ADC repeat mode code example. we will recommend not using multiple sample-and-conversion setting in the repeat mode.

**Attention** This is a public forum