This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP432E401Y: Can program GPIO PF4 as an output pin

Part Number: MSP-EXP432E401Y


I'm a newbie.  I am trying to use a timer to toggle a gpio pin.  I thought I read that PF4 can be used as an output GPIO pin.  So,  I added the following line to 

MSP_EXP432401Y.c

GPIO_PinConfig gpioPinConfigs[] = {

 ...

   GPIOMSP432E4_PF4 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_HIGH,

  ...

};

and in MSP_EXP432401Y.c  : typedef enum MSP_EXP432E401Y_GPIOName {

       MSP_EXP432E401Y_GPIO_PP4,

Well, the timer is working but instread of pin PF4 toggling, the LED on the board is toggling.

Lastly, in a similar manner as indicated above, I tried another GPIO pin,  PP4, and it does not seem to be toggling when view on an o scope.

Any help would be appreciated. 

**Attention** This is a public forum