This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/MSP-FET: MSP-FET issue

Part Number: MSP-FET
Other Parts Discussed in Thread: MSP430F6736, EVM430-F6736

Tool/software: TI C/C++ Compiler

Hi All,

What are the differences between MSP-FET products in 2014 and 2018?

We tested the following questions about the MSP-FET 14-pin JTAG connector.

1. The 2014 version of Pin 4 can be used as an open circuit when using external VCC, but the 2018 version of Pin 4 requires the use of cnnect to connect to the target board VCC.

2. EVM430-F6736 - MSP430F6736 EVM for Metering board on 2014 MSP-FET can use internal VCC to connected for debug but  the 2018 MSP-FET  requires the use of external VCC.

Thanks

HC.Huang

**Attention** This is a public forum