Other Parts Discussed in Thread: MSP430F2013
Hello Forum,
I am designing a AC lamp dimmer with MSP430F2013, i am referring to Appnote "controlling Triac with MSP430", Zero Cross Detection is made using 2 diodes and cap connected to a port pin, i have following doubts :
1) inside the External interrupt ISR can the trigger level be changed alternately like initially it will be high -to -low trigger and next trigger will happen on low-to-high level ?
2) i am using BT136-600 as triac in Quadrant 2&3 (gate low), does this scheme work with 3.3V VCC
3) can i parallel port pins to directly drive the Triac w/o using NPN transistor, is it safe for MSP430
Regards,
Nura