This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bootstrap loader G2332



Hello,

is there any information available which version of the bootstrap loader is implemented in the G2332? I could not find this information in user guide SLAU319A, yet.

If G2332 will have a version that is not described in the user guide, what differeces are tobe expected?

Thanks and best regards,
Philipp

  • Hi,

       Good point, I need to update the documentation.  As always, this will first go onto the BSL Wiki, then make it's way to the PDFs.  Basically, for this device I updated BSL version 2.02 (as seen on many other 2xx devices).  The BSL version was updated to 2.03 to reflect a small internal change required to move the TX/RX pins... but there should be zero external differences.

    update: To be clear, I believe this particular device is one of the value line devices without a BSL.  The above information applies to devices ending in a '3'

  • Hi Friend,

    I am also working on same kind of project in which Firmware Update by using UART by sending command through PC. I am making custom BSL ,now i am able to write data in flash and also program counter But when i am going to reset my code it is giving  "No source available for "0x00". i couldn't go my application code. please suggest me i need to erase Stack Memory / Stack Pointer .....?

**Attention** This is a public forum