Part Number: MSP432P401R
Hello,
I have a question.
I would like to run "voice_detection_demo_MSP_EXP432P401R_tirtos_ccs" .
But it doesn't work well.(The display turns white and the menu is not displayed)
Are there any possible factors?
I ran the demo following procedure as bellow.
1.Connect the jumper from J2-11 (labeled P3.6) to J2-17 (labeled P5.7) on the bottom of the MSP432 Launchpad Red
2.I use Kentec display, so two zero-ohm resistors installed in R1 and R4 on the Audio BoosterPack and no resistors placed in R3 and R5
3.From top to bottom, install Kentec Display, Audio BoosterPack, MSP432 Launchpad in layers
4.In CCS, I imported the project into the workspace with copied
5.Two predefined symbols, KENTEC and KENTEC_TOUCH, are defined at Predefined Symbols in Properties
6.Build the Project, then, there is no error.
7.Load and run the project
My environment is as bellow:
simplelink_sdk_voice_detection_plugin_1_50_00_15
simplelink_msp432p4_sdk_1_50_00_12(I also tried the latest simplelink_msp432p4_sdk_1 _ 60 _ 00 _ 12)
Code Composer Studio 7.4.0
Compiler TI v16.9.3. LTS
Regards,