Other Parts Discussed in Thread: MSP432E411Y
Hi guys,
Please redirect if I am in the wrong forum. My problem is that all help questions start with a part or product. I need help in choosing a product to start with.
I am looking for the MINIMAL processor to drive a 7" touchscreen with say, 800x600 resolution. This is for a benchtop automation project. I don't think I need a full up operating system. I don't want an embedded PC because there will only be a simple 2D graphics to splash onto the screen. The graphics will only be buttons, alphanumeric keypad, text display, and maybe a progress bar or other indicators of machine status. Once the user enters the parameters and presses "Start" the processor sends a serial data stream to another processor which actually runs the machine. So, other than taking in some parameters and displaying status, the processor running the graphics screen will just be sitting idle. I don't need the flexibility to run multiple programs as there will only be a single program- get the parameters and download the data.
Thanks for any input and I don't mind being given just a few links so I can do my own research.
Jim