Part Number: MSP430FR5994
Tool/software: Code Composer Studio
Hello There,
I have an issue incredibly similar to a previous situation [[View:https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/679007?tisearch=e2e-sitesearch&keymatch=MSP%20FET%20JTAG:1230:0]
], except our system's VCC is set to 1.8V (though, if this is too low we can move to 2V, though this would be the maximum). Our RC values are as follows:
R: 47 kOhm
C: 1500 pF
I can also add a few pictures if anything else is needed, though it is (as I stated above) very similar to the previous thread.
Thank you for your time, and I hope that all is well.
-Brad