Part Number: MSP-EXP430FR4133
Other Parts Discussed in Thread: MSP430FR4133, MSP-FET
Hi,
I am trying to use the BSL Scripter to connect with the BSL on the MSP430FR4133 chip present on the EXP430FR4133 board through the back channel uart but wothout success. The SPI-ByWire works fine.
I have seen a post that suggest to add PARITY to the MODE command but this do not solve my issue, nothing change with or without PARITY.
I start the BSL through manually keeping pressed the reset pushbutton (S3), then manually connecting the TST pin to the 3.3V (jumper removed from J101) for at least 2 times and then releasing the S3 button.
Then the BSL starts, because I see the TXD going HIGH and after the messages received from RXD, the TXD answers but getting the " [ACK_ERROR_MESSAGE]Header incorrect! " message.
So my first question is: What is wrong?
Other questions:
This EXP board can start the BSL like other tools do (RochetMSP430-BSL and/or by MSP-FET)?
What are the timing of the BSL sequence on RESET and TEST signal generated by RochetMSP430-BSL and/or by MSP-FET?
I need this information to dimension my translator driver speed in my final design and I have not such tools at the moment.
I hope they are not in the range 28ns to 15us because it should be quite fast. I hope they can be more far relaxed.
Thank you in advance.
Luca