Other Parts Discussed in Thread: MSP-EXP430FR5994
Tool/software: TI-RTOS
When I go to the TI-RTOS for MSP430 examples in the CCS in the Resource explorer and try to run some TI-RTOS project I always get this massage as output (in Console window):
MSP430: Flash/FRAM usage is 12143 bytes. RAM usage is 2736 bytes.
MSP430: AutoRun: Target not run as the symbol "main" is not defined
I get this massage too:
Break at address "0x0" with no debug information available, or outside of program code.
Build always completes successfully but I can not run the project. Can you tell me is there anything else that I need to do in order to run this TI-RTOS projects?
I'm using MSP430FR5994 and the project that doesn't work is MSP-EXP430FR5994\Driver Examples\Empty Examples\Empty Project.