Part Number: SIMPLELINK-MSP432-SDK
Tool/software: TI-RTOS
I am trying to post a semaphore from my UART HWI and I"m getting an exception:
My setup is as follow:
- CCS Version: 7.3.0.00019
- XDC Tools 3.50.5.12_core
- SimpleLink MSP432P4 SDK 2.10.0.14
- Ubuntu Virtual Box VM Development platform
- Older "Black" MSP432Pr401R Launchpad Eval Kit
ti.sysbios.knl.Task: line 424: E_spOutOfBounds: Task 0x200099f0 stack error, SP = 0x20008ac4. xdc.runtime.Error.raise: terminating execution
I believe this is because the the HWI's are running as zero-latency interrupts.
It seems like these interrupts also prevent me from passing a param into the HWI.
Is there any way I can disable the zero-latency interrupt for these, so I can make the OS Calls?
Cfg File Example:
/* ================ Hwi configuration ================ */
var halHwi = xdc.useModule('ti.sysbios.hal.Hwi');
var m3Hwi = xdc.useModule('ti.sysbios.family.arm.m3.Hwi');
/*
* Checks for Hwi (system) stack overruns while in the Idle loop.
*
* Pick one:
* - true (default)
* Checks the top word for system stack overflows during the idle loop and
* raises an Error if one is detected.
* - false
* Disabling the runtime check improves runtime performance and yields a
* reduced flash footprint.
*/
halHwi.checkStackFlag = true;
//halHwi.checkStackFlag = false;
/*
* The following options alter the system's behavior when a hardware exception
* is detected.
*
* Pick one:
* - Hwi.enableException = true
* This option causes the default m3Hwi.excHandlerFunc function to fully
* decode an exception and dump the registers to the system console.
* This option raises errors in the Error module and displays the
* exception in ROV.
* - Hwi.enableException = false
* This option reduces code footprint by not decoding or printing the
* exception to the system console.
* It however still raises errors in the Error module and displays the
* exception in ROV.
* - Hwi.excHandlerFunc = null
* This is the most aggressive option for code footprint savings; but it
* can difficult to debug exceptions. It reduces flash footprint by
* plugging in a default while(1) trap when exception occur. This option
* does not raise an error with the Error module.
*/
m3Hwi.enableException = true;
//m3Hwi.enableException = false;
//m3Hwi.excHandlerFunc = null;
/*
* Enable hardware exception generation when dividing by zero.
*
* Pick one:
* - 0 (default)
* Disables hardware exceptions when dividing by zero
* - 1
* Enables hardware exceptions when dividing by zero
*/
m3Hwi.nvicCCR.DIV_0_TRP = 0;
//m3Hwi.nvicCCR.DIV_0_TRP = 1;
/*
* Enable hardware exception generation for invalid data alignment.
*
* Pick one:
* - 0 (default)
* Disables hardware exceptions for data alignment
* - 1
* Enables hardware exceptions for data alignment
*/
m3Hwi.nvicCCR.UNALIGN_TRP = 0;
//m3Hwi.nvicCCR.UNALIGN_TRP = 1;
/***** Some Other Stuff ****/
halHwi.dispatcherAutoNestingSupport = false;
var halHwi0Params = new halHwi.Params();
halHwi0Params.instance.name = "hHwiEusciA2";
halHwi0Params.arg = 2;
halHwi0Params.enableInt = false;
halHwi0Params.priority = 3;
Program.global.hHwiEusciA2 = halHwi.create(34, "&Msp432UartIsrA2", halHwi0Params);
var halHwi1Params = new halHwi.Params();
halHwi1Params.instance.name = "hHwiEusciA0";
halHwi1Params.priority = 3;
halHwi1Params.enableInt = false;
Program.global.hHwiEusciA0 = halHwi.create(32, "&Msp432UartIsrA0", halHwi1Params);