This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6745: F674x(null) ADC 10 conversion with synchronized SD24_B

Expert 2355 points

Part Number: MSP430F6745

Hi,

SLAS768D Table 24 describes SD24_B trigger pulse can be trigger ADC10.

 http://www.ti.com/lit/ds/symlink/msp430f6779.pdf

Also U/G describes that on 29.2.12 Trigger Generator "Note"...

 Only the MSP430F674xx(1)(A), MSP430F676xx(1)(A), and MSP430F677x(1)(A) devices support the trigger generator.

 http://www.ti.com/lit/ug/slau208q/slau208q.pdf

 So, MSP430F674x(Null) device can be operate ADC 10 conversion with synchronized SD24_B?

 Regards,

 kyt

  • Hello,

    Yes, the MSP430F6745 supports the trigger generator feature of the SD24_B module. The values in the parenthesis after the part number indicate either a 1 or null and either an A or null after the main portion of the part number. I hope this helps!

    Regards,

    James

    MSP Customer Applications

**Attention** This is a public forum