Part Number: MSP430FR2532
Can the msp430fr2532 startup from 1.8 Volts if the SVS is disabled in the firmware? I would like to run the part at 1.8 volts since another processor in the system uses 1.8 volts to avoid level translators. The datasheet says it can run at 1.8 volts if SVS is turned off but SVS is turned on by default.