Part Number: MSP430F5329
I am getting a XT1LFOFFG fault in UCSCTL7
At start I think I should get it because "After a PUC, the UCS module default configuration is:
• XT1 in LF mode is selected as the oscillator source for XT1CLK. XT1CLK is selected for ACLK "
So I expect a fault,
So then I set ACLK to REFO with
UCS_initClockSignal(UCS_ACLK, UCS_REFOCLK_SELECT, UCS_CLOCK_DIVIDER_1 );
And Turn off XT1 with UCS_turnOffXT1();
So then I try to clear the flag:
if (UCSCTL7 & XT1LFOFFG) // If XTL LF Mode is set clear it, this is disabled
{
UCSCTL7 &= ~XT1LFOFFG; // clear it
}
And the XT1LFOFFG percists.
It says
| XT1 oscillator fault flag (LF mode). If this bit is set, the OFIFG flag is also set. XT1LFOFFG is set if a XT1 fault condition exists. XT1LFOFFG can be cleared by software. If the XT1 fault condition still remains, XT1LFOFFG is set. 0b = No fault condition occurred after the last reset. 1b = XT1 fault (LF mode). A XT1 fault occurred after the last reset. |
If it is off and ACLK is 32768 Hz from REFo
And SMCLK and MCLK are 7,372,800 Hz using the REFO as input to DCO FLL why is there a fault?
void CLK_Init(void)
{
uint16_t status;
// I believe when everything is done the clocks are:
// ACLK = 32768 Hz using REFO
// MCLK = 7,372,800 Hz from REFO
// SMCLK = 7,372,800 Hz from REFO
// Set DCO FLL reference = REFO
// Any external Crystals are off
_BIC_SR(SCG0); // Make sure the FLL is turned on.
UCS_initClockSignal(UCS_FLLREF,
UCS_REFOCLK_SELECT,
UCS_CLOCK_DIVIDER_1 );
// Set ACLK = REFO
UCS_initClockSignal(UCS_ACLK,
UCS_REFOCLK_SELECT,
UCS_CLOCK_DIVIDER_1 );
UCS_initClockSignal(UCS_SMCLK,
UCS_DCOCLKDIV_SELECT,
UCS_CLOCK_DIVIDER_1 );
// Set Ratio and Desired MCLK Frequency and initialize DCO
UCS_initFLLSettle(7373, // kHz
225 ); // 7372.8/32.768 = 225
// In this mode we are below 8 MHz so we can have PMMCOREV0 = 1.8V
// so now that the frequency is lower we can set the voltage.
status = PMM_setVCore(PMM_CORE_LEVEL_0);
if (status == STATUS_FAIL) while(1); // we have problems. When debugging stop here.
//PMM_enableSvsHSvmH(); // in this mode we have highside so turn on.
//PMM_enableSvsLSvmL(); // we need low side enabled in this mode.
//PMM_enableSvsLReset(); // We should never see a low voltage event
UCS_turnOffXT1(); // Make sure external 32.768 kHz Crystal is off
if (UCSCTL7 & XT1LFOFFG) // If XTL LF Mode is set clear it, this is disabled
{
UCSCTL7 &= ~XT1LFOFFG; // clear it
}
UCS_turnOffXT2(); // Make sure external 14.7456 MHz Crystal is off
//Verify if the Clock settings are as expected
clockValue[0] = UCS_getMCLK();
clockValue[1] = UCS_getSMCLK();
clockValue[2] = UCS_getACLK();
T1Enable_Port();
if (d.Debug[7]) print_clock_values();
return;
}