Other Parts Discussed in Thread: ENERGIA
Hello,
I am working on finding the resistor value of RC circuit. My idea was to start charging the RC circuit until (Tau~=RC) at 63 % of full voltage, and calculating the elapsed time , and from the reference capacitor we can get the value of the resistor.
I wrote the following code, however, what I get was not precise. The main problem I know it is with the timer, Can someone help me to modify my timer initialization to make precise measurements.
Thank you a lot
/* * This code is to measure resistor by charging and discharging capacitor * using one general timer * */ #include <msp430.h> #include <stdio.h> static unsigned int intervals=0; // Count number of 50,000 counts /** * main.c */ void main(void) { float StartTime=0; float ElapsedTime=0; float ResistorKohm,RefCapacitorNF=100;// capacitor in nano WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer PM5CTL0 = ~LOCKLPM5; //unlock the GPIO pins //set the clock CSCTL0_H = 0xA5; CSCTL1 |= DCOFSEL_6; // Set max. DCO setting = 8MHz CSCTL2 = SELA__VLOCLK + SELS_3 + SELM_3; CSCTL3 = DIVA__1 + DIVS__1 + DIVM__1; //Setting the timer for counting TA0CCR0 = 40000; // 40000 * 0.125us = 5000us = 5msec, where 1/8MHZ=0.125us TA0CTL = TASSEL__SMCLK + MC__UP; // Set SMCLK, UP mode TA0CCTL0 = CCIE; // Enable interrupt for Timer_0 _BIS_SR(GIE); // Activate interrupts previously enabled //Setting up the pins P1DIR |= BIT3; // Set P1.3 as output to charge capacitor P1OUT &= ~BIT3; // Clear port1 P1SEL1 |= BIT5; // Configure P1.5 for ADC P1SEL0 |= BIT5; // Configure ADC12 ADC12CTL0 = ADC12SHT0_2 | ADC12ON; // Sampling time, S&H=16, ADC12 on ADC12CTL1 = ADC12SHP; // Use sampling timer ADC12CTL2 |= ADC12RES_2; // 12-bit conversion results ADC12MCTL0 |=ADC12INCH_5; // A5 ADC input select(P1.5) while(1) { ADC12CTL0 |= ADC12ENC; // Enable conversion ADC12CTL0 |= ADC12SC;// Start conversion P1OUT|=BIT3; StartTime=((intervals*40000)+TA0R)*0.125; while(ADC12MEM0 < 2889) { ADC12CTL0 |= ADC12SC;// Start conversion } // the value is 63.2% of full ADC range =2889 ElapsedTime=(((intervals*40000)+TA0R)*0.125)-StartTime; ResistorKohm=ElapsedTime/RefCapacitorNF; printf("\n this is start time: %2.2f",StartTime); printf("\n this is elapsedtime: %2.2f",ElapsedTime); printf("\n the resistor : %8.3f",ResistorKohm); P1OUT &= ~BIT3; __delay_cycles(1000000); } } //************************************************************************ // Timer0 Interrupt Service Routine //************************************************************************ #pragma vector=TIMER0_A0_VECTOR __interrupt void Timer0_ISR (void) { intervals = intervals + 1; // Update number of TA0CCR0 counts }